SimulationOptionsBuilderStationary Enumeration¶
NXOpen.CAM.SimulationOptionsBuilder.Stationary is an alias for NXOpen.CAM.SimulationOptionsBuilderStationary
-
class
NXOpen.CAM.
SimulationOptionsBuilderStationary
¶ Bases:
object
The stationary options
Enum Members
Enum Member Enum Member Description Eath use earth stationaryPart use part stationaryTool use tool stationary-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-