SimulationOptionsBuilderSimulationDisplayMode Enumeration¶
NXOpen.CAM.SimulationOptionsBuilder.SimulationDisplayMode is an alias for NXOpen.CAM.SimulationOptionsBuilderSimulationDisplayMode
-
class
NXOpen.CAM.
SimulationOptionsBuilderSimulationDisplayMode
¶ Bases:
object
The modes of the simulation display. - :py:class:` NXOpen.CAM.SimulationOptionsBuilderSimulationDisplayMode.SuppressAll < NXOpen.CAM.SimulationOptionsBuilderSimulationDisplayMode>` will suppress display updates in graphics windows and NC program in Simulation Control Panel. - :py:class:` NXOpen.CAM.SimulationOptionsBuilderSimulationDisplayMode.SuppressGraphics < NXOpen.CAM.SimulationOptionsBuilderSimulationDisplayMode>` will suppress display updates in graphics windows. - :py:class:` NXOpen.CAM.SimulationOptionsBuilderSimulationDisplayMode.All < NXOpen.CAM.SimulationOptionsBuilderSimulationDisplayMode>` will show all display updates in graphics windows and NC program in Simulation Control Panel.
Enum Members
Enum Member Enum Member Description SuppressAll suppress graphics and NC program updatesSuppressGraphics suppress graphics updatesAll show all-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-