RoundPointBuilderOutput Enumeration

NXOpen.CAM.RoundPointBuilder.Output is an alias for NXOpen.CAM.RoundPointBuilderOutput

class NXOpen.CAM.RoundPointBuilderOutput

Bases: object

the decimal places

Enum Members

Enum Member Enum Member Description
NoRounding
No Rounding
Thousand
nearest thousand
Hundred
nearest hundred
Ten
nearest ten
One
no decimals
Tenth
nearest tenth
Hundredth
nearest hundredth
Thousandth
nearest thousandth
TenThousandth
nearest ten thousandth
HundredThousandth
nearest hundred thousandth
Millionth
nearest millionth
TenMillionth
nearest ten millionth
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.