RoughFinishTurningBuilderRegionSelectionTypes Enumeration

NXOpen.CAM.RoughFinishTurningBuilder.RegionSelectionTypes is an alias for NXOpen.CAM.RoughFinishTurningBuilderRegionSelectionTypes

class NXOpen.CAM.RoughFinishTurningBuilderRegionSelectionTypes

Bases: object

the Region Selection types

Enum Members

Enum Member Enum Member Description
Automatic
Automatic cut region selection.
Manual
Manual cut region selection.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.