RoughFinishTurningBuilderMinmaxSizeUnits Enumeration

NXOpen.CAM.RoughFinishTurningBuilder.MinmaxSizeUnits is an alias for NXOpen.CAM.RoughFinishTurningBuilderMinmaxSizeUnits

class NXOpen.CAM.RoughFinishTurningBuilderMinmaxSizeUnits

Bases: object

the Minimum/Maximum Size Axial/Radial units

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Length
Length.
Percentage
Percentage
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.