RoughFinishTurningBuilderMinmaxAreaUnits Enumeration

NXOpen.CAM.RoughFinishTurningBuilder.MinmaxAreaUnits is an alias for NXOpen.CAM.RoughFinishTurningBuilderMinmaxAreaUnits

class NXOpen.CAM.RoughFinishTurningBuilderMinmaxAreaUnits

Bases: object

the Minimum/Maximum Area units

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Square
Square length.
Percentage
Percentage
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.