RoughFinishTurningBuilderExtendModeTypes Enumeration

NXOpen.CAM.RoughFinishTurningBuilder.ExtendModeTypes is an alias for NXOpen.CAM.RoughFinishTurningBuilderExtendModeTypes

class NXOpen.CAM.RoughFinishTurningBuilderExtendModeTypes

Bases: object

the Extend Mode types

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Specify
Specify
Tagential
Tagential
Tangential
Tangential
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.