RoughFinishTurningBuilderCustomMemberDataTypes Enumeration

NXOpen.CAM.RoughFinishTurningBuilder.CustomMemberDataTypes is an alias for NXOpen.CAM.RoughFinishTurningBuilderCustomMemberDataTypes

class NXOpen.CAM.RoughFinishTurningBuilderCustomMemberDataTypes

Bases: object

the Custom Member Data types

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
WithinRegion
Within Region
WithinDistance
Within Distance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.