ReliefPlunge Class

class NXOpen.CAM.ReliefPlunge

Bases: NXOpen.TaggedObject

Represents a NXOpen.CAM.ReliefPlunge

New in version NX6.0.0.

Properties

Property Description
Distance Returns or sets the relief plunge distance
Tag Returns the Tag for this object.
Type Returns or sets the relief plunge type
Unit Returns or sets the relief plunge unit

Methods

Enumerations

ReliefPlungeTypes Enumeration the relief plunge options
ReliefPlungeUnitTypes Enumeration the relief plunge options

Property Detail

Distance

ReliefPlunge.Distance

Returns or sets the relief plunge distance

-------------------------------------

Getter Method

Signature Distance()

Returns:the relief plunge distance
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Distance(distance)

Parameters:distance (float) – the relief plunge distance

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Type

ReliefPlunge.Type

Returns or sets the relief plunge type

-------------------------------------

Getter Method

Signature Type()

Returns:the relief plunge mode
Return type:NXOpen.CAM.ReliefPlungeTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(reliefPlungeValue)

Parameters:reliefPlungeValue (NXOpen.CAM.ReliefPlungeTypes) – the relief plunge mode

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Unit

ReliefPlunge.Unit

Returns or sets the relief plunge unit

-------------------------------------

Getter Method

Signature Unit()

Returns:the relief plunge unit
Return type:NXOpen.CAM.ReliefPlungeUnitTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Unit(reliefPlungeUnit)

Parameters:reliefPlungeUnit (NXOpen.CAM.ReliefPlungeUnitTypes) – the relief plunge unit

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)