RampingModeTypes Enumeration

NXOpen.CAM.RampingMode.Types is an alias for NXOpen.CAM.RampingModeTypes

class NXOpen.CAM.RampingModeTypes

Bases: object

the ramping mode options

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
RampOutOnEveryOtherPass
Ramping mode: Ramp Out on every other Pass
RampInOnEveryOtherPass
Ramping mode: Ramp In on every other Pass
RampOutFirst
Ramping mode: Ramp Out first
RampInFirst
Ramping mode: Ramp In first
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.