ProbeInspectBorebossMoveBuilderGeometry Enumeration

NXOpen.CAM.ProbeInspectBorebossMoveBuilder.Geometry is an alias for NXOpen.CAM.ProbeInspectBorebossMoveBuilderGeometry

class NXOpen.CAM.ProbeInspectBorebossMoveBuilderGeometry

Bases: object

the geometry type

Enum Members

Enum Member Enum Member Description
Cylinder
Cylinder
Point
Point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.