ProbeInspectBorebossMoveBuilderAngle Enumeration

NXOpen.CAM.ProbeInspectBorebossMoveBuilder.Angle is an alias for NXOpen.CAM.ProbeInspectBorebossMoveBuilderAngle

class NXOpen.CAM.ProbeInspectBorebossMoveBuilderAngle

Bases: object

the angle type

Enum Members

Enum Member Enum Member Description
Predefined
Predefined angles
Custom
Custom angles
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.