PreprocessGeometryBuilder Class¶
-
class
NXOpen.CAM.
PreprocessGeometryBuilder
¶ Bases:
NXOpen.Builder
Represents a Preprocess Geometry Builder
To create a new instance of this class, use
NXOpen.CAM.CAMSetup.CreatePreprocessGeometryBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
FixedVector | Returns or sets the default tool axis vector |
Tag | Returns the Tag for this object. |
TriangleTolerance | Returns or sets the default triangle tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Create | Create new facet body |
Delete | Delete one facet body |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetObjects | Get solid bodies and relevant facet bodies |
GetParameter | Get tolerance and vector of facet body which is gotten from relevant solid body |
SetParameter | Set tolerance and vector for facet body which is gotten from relevant solid body |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FixedVector¶
-
PreprocessGeometryBuilder.
FixedVector
¶ Returns or sets the default tool axis vector
-------------------------------------
Getter Method
Signature
FixedVector()
Returns: Return type: NXOpen.SmartObject
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
FixedVector(newVector)
Parameters: newVector ( NXOpen.SmartObject
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TriangleTolerance¶
-
PreprocessGeometryBuilder.
TriangleTolerance
¶ Returns or sets the default triangle tolerance
-------------------------------------
Getter Method
Signature
TriangleTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
TriangleTolerance(tolerance)
Parameters: tolerance (float) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Create¶
-
PreprocessGeometryBuilder.
Create
¶ Create new facet body
Signature
Create(obj, tolerance, vector)
Parameters: - obj (
NXOpen.NXObject
) – the new solid body, it will be converted to facet body in function - tolerance (float) – tolerance
- vector (
NXOpen.NXObject
) – vector
New in version NX6.0.0.
License requirements: None.
- obj (
Delete¶
-
PreprocessGeometryBuilder.
Delete
¶ Delete one facet body
Signature
Delete(obj)
Parameters: obj ( NXOpen.NXObject
) – the solid body,its relevant facet body will be deleted actuallyNew in version NX6.0.0.
License requirements: None.
GetObjects¶
-
PreprocessGeometryBuilder.
GetObjects
¶ Get solid bodies and relevant facet bodies
Signature
GetObjects()
Returns: a tuple Return type: A tuple consisting of (solidBodies, facetBodies). solidBodies is a list of NXOpen.NXObject
. the solid bodies facetBodies is a list ofNXOpen.NXObject
. the facet bodies, corresponding to facet bodiesNew in version NX6.0.0.
License requirements: None.
GetParameter¶
-
PreprocessGeometryBuilder.
GetParameter
¶ Get tolerance and vector of facet body which is gotten from relevant solid body
Signature
GetParameter(obj)
Parameters: obj ( NXOpen.NXObject
) – the solid body,will find relevant facet body dependent on itReturns: a tuple Return type: A tuple consisting of (tolerance, vector). tolerance is a float. tolerance vector is a NXOpen.NXObject
. vectorNew in version NX6.0.0.
License requirements: None.
SetParameter¶
-
PreprocessGeometryBuilder.
SetParameter
¶ Set tolerance and vector for facet body which is gotten from relevant solid body
Signature
SetParameter(obj, tolerance, vector)
Parameters: - obj (
NXOpen.NXObject
) – the solid body,will find relevant facet body dependent on it - tolerance (float) – tolerance
- vector (
NXOpen.NXObject
) – vector
New in version NX6.0.0.
License requirements: None.
- obj (
Validate¶
-
PreprocessGeometryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.