PathLevelMarker Class¶
-
class
NXOpen.CAM.
PathLevelMarker
¶ Bases:
NXOpen.TransientObject
This class represents the data of a Linear Motion
New in version NX10.0.3.
Properties¶
Property | Description |
---|---|
LevelDepth | Returns or sets the level depth |
LevelNormal | Returns or sets the level normal |
Property Detail¶
LevelDepth¶
-
PathLevelMarker.
LevelDepth
¶ Returns or sets the level depth
-------------------------------------
Getter Method
Signature
LevelDepth()
Returns: Return type: float New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
LevelDepth(levelDepth)
Parameters: levelDepth (float) – New in version NX10.0.3.
License requirements: None.
LevelNormal¶
-
PathLevelMarker.
LevelNormal
¶ Returns or sets the level normal
-------------------------------------
Getter Method
Signature
LevelNormal()
Returns: Return type: NXOpen.Vector3d
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
LevelNormal(levelNormal)
Parameters: levelNormal ( NXOpen.Vector3d
) –New in version NX10.0.3.
License requirements: None.
Method Detail¶
Dispose¶
-
PathLevelMarker.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX10.0.3.
License requirements: None.