PathLaserPowderData Class¶
-
class
NXOpen.CAM.
PathLaserPowderData
¶ Bases:
NXOpen.TransientObject
Definition for Laser powder data
New in version NX9.0.3.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetMaterial | Get the powder material @return |
Method Detail¶
Dispose¶
-
PathLaserPowderData.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX9.0.3.
License requirements: None.