PathHelixMotion Class¶
-
class
NXOpen.CAM.
PathHelixMotion
¶ Bases:
NXOpen.CAM.PathCircularMotion
This class represents the data of a Linear Motion
New in version NX10.0.1.
Properties¶
Property | Description |
---|---|
ArcAxis | Returns or sets the axis of the arc motion |
ArcCenter | Returns or sets the center of the arc motion |
ArcRadius | Returns or sets the radius of the arc motion |
Direction | Returns or sets the direction of the arc motion |
EndPoint | Returns or sets the end point of the motion |
IsCustomFeedrate | Returns or sets the custom feed rate indicator |
MotionType | Returns or sets the motion type |
NumberOfRevolutions | Returns or sets the motion type |
ToolAxis | Returns or sets the tool axis of the motion |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetFeedrate | Get feed rate information |
SetFeedrate | Set feed rate information. |
Property Detail¶
NumberOfRevolutions¶
-
PathHelixMotion.
NumberOfRevolutions
¶ Returns or sets the motion type
-------------------------------------
Getter Method
Signature
NumberOfRevolutions()
Returns: Return type: float New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfRevolutions(numOfRevolutions)
Parameters: numOfRevolutions (float) – New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)