ParamValueIntent Enumeration

class NXOpen.CAM.ParamValueIntent

Bases: object

The source of values for design logic enum component within status components

New in version NX5.0.0.

Enum Members

Enum Member Enum Member Description
PartUnits
value used as is
ToolDep
value is percent of tool
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.