OperationCollectionUseDefaultName Enumeration

NXOpen.CAM.OperationCollection.UseDefaultName is an alias for NXOpen.CAM.OperationCollectionUseDefaultName

class NXOpen.CAM.OperationCollectionUseDefaultName

Bases: object

Whether use the default name in creation

Enum Members

Enum Member Enum Member Description
False
don’t user the default name
True
use the default name
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.