OperationBuilderOptimizationLevelTypes Enumeration

NXOpen.CAM.OperationBuilder.OptimizationLevelTypes is an alias for NXOpen.CAM.OperationBuilderOptimizationLevelTypes

class NXOpen.CAM.OperationBuilderOptimizationLevelTypes

Bases: object

Available types for optimization level in operation

Enum Members

Enum Member Enum Member Description
Standard
standard
Advanced
advanced
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.