OperationBuilderOptimizationBasedOnTypes Enumeration

NXOpen.CAM.OperationBuilder.OptimizationBasedOnTypes is an alias for NXOpen.CAM.OperationBuilderOptimizationBasedOnTypes

class NXOpen.CAM.OperationBuilderOptimizationBasedOnTypes

Bases: object

Available types for optimization based on in operation

Enum Members

Enum Member Enum Member Description
Dist
dist
Orient
orient
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.