OperationBuilderHoleDepthTypes Enumeration

NXOpen.CAM.OperationBuilder.HoleDepthTypes is an alias for NXOpen.CAM.OperationBuilderHoleDepthTypes

class NXOpen.CAM.OperationBuilderHoleDepthTypes

Bases: object

Available types for Hole Depth Type in feature milling and hole making

Enum Members

Enum Member Enum Member Description
Point
Smart Point
Rule
Depth/Rule
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.