OperationBuilderHoleAxisTypes Enumeration

NXOpen.CAM.OperationBuilder.HoleAxisTypes is an alias for NXOpen.CAM.OperationBuilderHoleAxisTypes

class NXOpen.CAM.OperationBuilderHoleAxisTypes

Bases: object

Available types for Hole Axis Type in feature milling and hole making

Enum Members

Enum Member Enum Member Description
Vector
Vector
Rule
Rule
RuleIfNoVector
Rule if no vector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.