NormalToToolAxisMoveBuilderOrientation Enumeration

NXOpen.CAM.NormalToToolAxisMoveBuilder.Orientation is an alias for NXOpen.CAM.NormalToToolAxisMoveBuilderOrientation

class NXOpen.CAM.NormalToToolAxisMoveBuilderOrientation

Bases: object

the normal orientation

Enum Members

Enum Member Enum Member Description
AlongVector
Along Vector
TowardsPoint
Towards Point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.