NcmctPartMountingBuilderPositioningTypes Enumeration¶
NXOpen.CAM.NcmctPartMountingBuilder.PositioningTypes is an alias for NXOpen.CAM.NcmctPartMountingBuilderPositioningTypes
-
class
NXOpen.CAM.
NcmctPartMountingBuilderPositioningTypes
¶ Bases:
object
Available types for positioning
Enum Members
Enum Member Enum Member Description OrientMachineZeroToMainMcs Orient Machine Zero to main MCSUseAssemblyPositioning Use Assembly PositioningUsePartMountJunction Use Part Mount JunctionUseOldMachineTransformation Use Old Machine TransformationKeepAssemblyConstraints Keep Assembly Constraints-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-