NcmWedmBuilderNonTiltLeadInTypes Enumeration

NXOpen.CAM.NcmWedmBuilder.NonTiltLeadInTypes is an alias for NXOpen.CAM.NcmWedmBuilderNonTiltLeadInTypes

class NXOpen.CAM.NcmWedmBuilderNonTiltLeadInTypes

Bases: object

the types available for non-tilt lead in

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Zm
non-tilt lead in type zm
FourAxis
non-tilt lead in type 4-axis
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.