NcmWedmBuilderLeadOutSameAsLeadInTypes Enumeration

NXOpen.CAM.NcmWedmBuilder.LeadOutSameAsLeadInTypes is an alias for NXOpen.CAM.NcmWedmBuilderLeadOutSameAsLeadInTypes

class NXOpen.CAM.NcmWedmBuilderLeadOutSameAsLeadInTypes

Bases: object

the types available for lead out same as lead in

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
No
not the same
Yes
the same as lead in
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.