NcmWedmBuilderLeadOutMethodTypes Enumeration

NXOpen.CAM.NcmWedmBuilder.LeadOutMethodTypes is an alias for NXOpen.CAM.NcmWedmBuilderLeadOutMethodTypes

class NXOpen.CAM.NcmWedmBuilderLeadOutMethodTypes

Bases: object

the types available for lead out method

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
SameAsLeadIn
same as lead in
Direct
direct lead out
Angular
angular lead out
Circular
circular lead out
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.