NcmWedmBuilderGlobalStopPointTypes Enumeration

NXOpen.CAM.NcmWedmBuilder.GlobalStopPointTypes is an alias for NXOpen.CAM.NcmWedmBuilderGlobalStopPointTypes

class NXOpen.CAM.NcmWedmBuilderGlobalStopPointTypes

Bases: object

the types available for wedm stop points

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Opstop
stop points option opstop
Stop
stop points option stop
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.