NcmWedmBuilderCutcomOnTypes Enumeration¶
NXOpen.CAM.NcmWedmBuilder.CutcomOnTypes is an alias for NXOpen.CAM.NcmWedmBuilderCutcomOnTypes
-
class
NXOpen.CAM.
NcmWedmBuilderCutcomOnTypes
¶ Bases:
object
the types available for cutcom on
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description NotSet no cutcom onBeforeLeadIn cutcom on before lead inAfterLeadIn cutcom on after lead inAtThreadPoint cutcom on at thread point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-