NcmTurnThreadBuilderLocalReturnMainModes Enumeration

NXOpen.CAM.NcmTurnThreadBuilder.LocalReturnMainModes is an alias for NXOpen.CAM.NcmTurnThreadBuilderLocalReturnMainModes

class NXOpen.CAM.NcmTurnThreadBuilderLocalReturnMainModes

Bases: object

The Local Return Main modes options

New in version NX8.5.0.

Enum Members

Enum Member Enum Member Description
Opstop
Opstop
ThreadPasses
Thread Passes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.