NcmTransferTypes Class¶
-
class
NXOpen.CAM.
NcmTransferTypes
¶ Bases:
NXOpen.TaggedObject
Represents a
CAM.NcmTransferTypes
New in version NX10.0.1.
Properties¶
Property | Description |
---|---|
FinalSafeDistance | Returns the final safe distance builder (inheritable tool dep) |
FinalType | Returns or sets the final type |
InitialSafeDistance | Returns the initial safe distance builder (inheritable tool dep) |
InitialType | Returns or sets the initial type |
Tag | Returns the Tag for this object. |
TransferInitialFinal | Returns the transfer settings for initial and final |
Methods¶
Enumerations¶
NcmTransferTypesFinalTypes Enumeration | Available types for final clearance in hole machining |
NcmTransferTypesInitialTypes Enumeration | Available types for initial clearance in hole machining |
Property Detail¶
FinalSafeDistance¶
-
NcmTransferTypes.
FinalSafeDistance
¶ Returns the final safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
FinalSafeDistance()
Returns: The final safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX10.0.1.
License requirements: None.
FinalType¶
-
NcmTransferTypes.
FinalType
¶ Returns or sets the final type
-------------------------------------
Getter Method
Signature
FinalType()
Returns: Return type: NXOpen.CAM.NcmTransferTypesFinalTypes
New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FinalType(finalType)
Parameters: finalType ( NXOpen.CAM.NcmTransferTypesFinalTypes
) –New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
InitialSafeDistance¶
-
NcmTransferTypes.
InitialSafeDistance
¶ Returns the initial safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
InitialSafeDistance()
Returns: The initial safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX10.0.1.
License requirements: None.
InitialType¶
-
NcmTransferTypes.
InitialType
¶ Returns or sets the initial type
-------------------------------------
Getter Method
Signature
InitialType()
Returns: Return type: NXOpen.CAM.NcmTransferTypesInitialTypes
New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialType(initialType)
Parameters: initialType ( NXOpen.CAM.NcmTransferTypesInitialTypes
) –New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
TransferInitialFinal¶
-
NcmTransferTypes.
TransferInitialFinal
¶ Returns the transfer settings for initial and final
-------------------------------------
Getter Method
Signature
TransferInitialFinal()
Returns: The transfer builder Return type: NXOpen.CAM.NcmTransferBuilder
New in version NX10.0.1.
License requirements: None.