NcmTransferBuilderTraverseTypes Enumeration¶
NXOpen.CAM.NcmTransferBuilder.TraverseTypes is an alias for NXOpen.CAM.NcmTransferBuilderTraverseTypes
-
class
NXOpen.CAM.
NcmTransferBuilderTraverseTypes
¶ Bases:
object
Available types for traverse
Enum Members
Enum Member Enum Member Description Same traverse setting from between regionsShortestToClearance traverse shortest to clearanceLowestSafeZ traverse at lowest safe zDirect traverse directSmooth traverse smooth spline-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-