NcmTransferBuilderLongMotionTypes Enumeration

NXOpen.CAM.NcmTransferBuilder.LongMotionTypes is an alias for NXOpen.CAM.NcmTransferBuilderLongMotionTypes

class NXOpen.CAM.NcmTransferBuilderLongMotionTypes

Bases: object

Available motion types for smooth

Enum Members

Enum Member Enum Member Description
Stepover
stepover smooth motion type
RetractTraverseEngage
retract traverse engage smooth motion type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.