NcmTransferBuilderAppDepToolAxisOptions Enumeration

NXOpen.CAM.NcmTransferBuilder.AppDepToolAxisOptions is an alias for NXOpen.CAM.NcmTransferBuilderAppDepToolAxisOptions

class NXOpen.CAM.NcmTransferBuilderAppDepToolAxisOptions

Bases: object

Available options for tool axis behavior

Enum Members

Enum Member Enum Member Description
NoChange
tool axis remains unchanged
Specify
tool axis as specified
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.