NcmTransfer Class¶
-
class
NXOpen.CAM.
NcmTransfer
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.NcmTransfer
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ApplySafetyToDirect | Returns or sets the apply safety to direct value |
MaxToolAxisChange | Returns or sets the max tool axis change |
SafeDistanceBuilder | Returns the transfer between regions safe distance builder (inheritable tool dep) |
Tag | Returns the Tag for this object. |
Type | Returns or sets the transfer between levels type |
Methods¶
Enumerations¶
NcmTransferTransferTypes Enumeration | Available types for transfer between regions in planar milling |
Property Detail¶
ApplySafetyToDirect¶
-
NcmTransfer.
ApplySafetyToDirect
¶ Returns or sets the apply safety to direct value
-------------------------------------
Getter Method
Signature
ApplySafetyToDirect()
Returns: the apply safety value Return type: bool New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplySafetyToDirect(applySafety)
Parameters: applySafety (bool) – the apply safety value New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
MaxToolAxisChange¶
-
NcmTransfer.
MaxToolAxisChange
¶ Returns or sets the max tool axis change
-------------------------------------
Getter Method
Signature
MaxToolAxisChange()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxToolAxisChange(newValue)
Parameters: newValue (float) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
SafeDistanceBuilder¶
-
NcmTransfer.
SafeDistanceBuilder
¶ Returns the transfer between regions safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
SafeDistanceBuilder()
Returns: The transfer between regions safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
Type¶
-
NcmTransfer.
Type
¶ Returns or sets the transfer between levels type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAM.NcmTransferTransferTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(transferType)
Parameters: transferType ( NXOpen.CAM.NcmTransferTransferTypes
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)