NcmScBuilderSmoothingOptions Enumeration

NXOpen.CAM.NcmScBuilder.SmoothingOptions is an alias for NXOpen.CAM.NcmScBuilderSmoothingOptions

class NXOpen.CAM.NcmScBuilderSmoothingOptions

Bases: object

Available options for smoothing behavior

Enum Members

Enum Member Enum Member Description
On
transfer smoothing activated
Off
transfer smoothing deactivated
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.