NcmPlanarEngRetBuilderMeasureHeightFrom Enumeration

NXOpen.CAM.NcmPlanarEngRetBuilder.MeasureHeightFrom is an alias for NXOpen.CAM.NcmPlanarEngRetBuilderMeasureHeightFrom

class NXOpen.CAM.NcmPlanarEngRetBuilderMeasureHeightFrom

Bases: object

Available types for the Height From which engage helical/ramp/plunge is measured in Planar Milling

Enum Members

Enum Member Enum Member Description
CurrentLevel
Measure from current level
PreviousLevel
Measure from previous level
Plane
Measure from user-defined plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.