NcmPlanarEngRetBuilderEngRetTypes Enumeration¶
NXOpen.CAM.NcmPlanarEngRetBuilder.EngRetTypes is an alias for NXOpen.CAM.NcmPlanarEngRetBuilderEngRetTypes
-
class
NXOpen.CAM.
NcmPlanarEngRetBuilderEngRetTypes
¶ Bases:
object
Available types for engage/retract in Planar Milling
Enum Members
Enum Member Enum Member Description SameAsDefault Same as Default (Inherit)SameAsClosed Same as Closed Engage (from open)SameAsEngage Same as (Open) Engage (from retract)Helical Helical RampRampOnShape Ramp on shapeZigzagRamp ZigZag RampLinear LinearArc ArcArcParallelToToolAxis Arc - Parallel to Tool AxisArcNormalToToolAxis Arc - Normal to Tool AxisArcNormalToPart Arc - Normal to PartHighSpeedArc High Speed ArcsPoints to-from pointsPlungeLift Plunge Engage/Lift RetractAlongVector Vector DistAngAngPlane Linear to planeVectorPlane Vector to planeNotSet NoneLinearRelativeCut Linear relative to cut directionSmooth Smooth-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-