NcmPlanarBuilderTransferBetweenRegionsTypes Enumeration

NXOpen.CAM.NcmPlanarBuilder.TransferBetweenRegionsTypes is an alias for NXOpen.CAM.NcmPlanarBuilderTransferBetweenRegionsTypes

class NXOpen.CAM.NcmPlanarBuilderTransferBetweenRegionsTypes

Bases: object

Available types for transfer between regions in planar milling

Enum Members

Enum Member Enum Member Description
Clearance
tool axis to clearance
PrevPlane
previous plane
Direct
direct
LowestSafeZ
lowest safe z
BlankPlane
Blank Plane
ShortestToClearance
shortest to clearance
CutPlaneToClearance
cut plane to clearance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.