NcmPlanarBuilderTransferBetweenLevelsTypes Enumeration

NXOpen.CAM.NcmPlanarBuilder.TransferBetweenLevelsTypes is an alias for NXOpen.CAM.NcmPlanarBuilderTransferBetweenLevelsTypes

class NXOpen.CAM.NcmPlanarBuilderTransferBetweenLevelsTypes

Bases: object

Available types for transfer between levels in planar milling

Enum Members

Enum Member Enum Member Description
PrevPlane
previous plane
Direct
direct
Clearance
clearance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.