NcmLaserEngageType Enumeration

NXOpen.CAM.NcmLaserEngage.Type is an alias for NXOpen.CAM.NcmLaserEngageType

class NXOpen.CAM.NcmLaserEngageType

Bases: object

the Engage Type enum

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
LinearRelToCut
linear - Relative to Cut
Arc
arc
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.