NcmHoleMachiningEngRet Class

class NXOpen.CAM.NcmHoleMachiningEngRet

Bases: NXOpen.TaggedObject

Represents a builder for an inheritable double value in of a CAM.

CAMObject .. versionadded:: NX7.5.0

Properties

Property Description
EngRetType Returns or sets the type of engage/retract
Height Returns the engage/retract height builder
MinClearance Returns the engage/retract min clearance builder
StartFromCenter Returns or sets the engage/retract start at arc center
Tag Returns the Tag for this object.

Methods

Enumerations

NcmHoleMachiningEngRetEngRetTypes Enumeration Available types for engage/retract in Planar Milling

Property Detail

EngRetType

NcmHoleMachiningEngRet.EngRetType

Returns or sets the type of engage/retract

-------------------------------------

Getter Method

Signature EngRetType()

Returns:the current value
Return type:NXOpen.CAM.NcmHoleMachiningEngRetEngRetTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EngRetType(engRetType)

Parameters:engRetType (NXOpen.CAM.NcmHoleMachiningEngRetEngRetTypes) – the new value

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

Height

NcmHoleMachiningEngRet.Height

Returns the engage/retract height builder

-------------------------------------

Getter Method

Signature Height()

Returns:The component builder
Return type:NXOpen.CAM.InheritableToolDepBuilder

New in version NX7.5.0.

License requirements: None.

MinClearance

NcmHoleMachiningEngRet.MinClearance

Returns the engage/retract min clearance builder

-------------------------------------

Getter Method

Signature MinClearance()

Returns:The component builder
Return type:NXOpen.CAM.InheritableToolDepBuilder

New in version NX7.5.0.

License requirements: None.

StartFromCenter

NcmHoleMachiningEngRet.StartFromCenter

Returns or sets the engage/retract start at arc center

-------------------------------------

Getter Method

Signature StartFromCenter()

Returns:the start from center
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StartFromCenter(startFromCenter)

Parameters:startFromCenter (bool) – the start from center

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)