NcmAvoidancePointBuilderPointStates Enumeration¶
NXOpen.CAM.NcmAvoidancePointBuilder.PointStates is an alias for NXOpen.CAM.NcmAvoidancePointBuilderPointStates
-
class
NXOpen.CAM.
NcmAvoidancePointBuilderPointStates
¶ Bases:
object
the types available for avoidance point definition
Enum Members
Enum Member Enum Member Description NotSet Avoidance point inactiveUseOther use from point (only for GoHome point)NoPoint use no point (only for GoHome point)UsePoint use specified point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-