MultipleStepoverBuilder Class

class NXOpen.CAM.MultipleStepoverBuilder

Bases: NXOpen.Builder

Represents a Builder which holds the data for a set of individual number of passes and stepover distance.

This is an abstract class and cannot be instantiated.

New in version NX6.0.0.

Properties

Property Description
Tag Returns the Tag for this object.

Methods

Method Description
Add Add a new item
Commit Commits any edits that have been applied to the builder.
Delete Delete a item
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetData Get item for the specified stepover index
GetNumberOfStepovers Get number of stepovers @return the number of stepover
GetObject Returns the object currently being edited by this builder.
Modify Modify item
MoveDown Move down a item
MoveUp Move up a item
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Add

MultipleStepoverBuilder.Add

Add a new item

Signature Add(indexAfter, numOfPasses, distance, intent)

Parameters:
  • indexAfter (int) – the index which new item will be added after
  • numOfPasses (int) – the num of passes for new item
  • distance (float) – the distance for new item
  • intent (int) – the intent for new item

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Delete

MultipleStepoverBuilder.Delete

Delete a item

Signature Delete(index)

Parameters:index (int) – the index of item to be deleted

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

GetData

MultipleStepoverBuilder.GetData

Get item for the specified stepover index

Signature GetData(index)

Parameters:index (int) – the index of item to be modified
Returns:a tuple
Return type:A tuple consisting of (numOfPasses, distance, intent). numOfPasses is a int. the new value of num of passes distance is a float. the new value of distance intent is a int. the new value of intent

New in version NX7.5.3.

License requirements: cam_base (“CAM BASE”)

GetNumberOfStepovers

MultipleStepoverBuilder.GetNumberOfStepovers

Get number of stepovers

Signature GetNumberOfStepovers()

Returns:the number of stepover
Return type:int

New in version NX7.5.3.

License requirements: cam_base (“CAM BASE”)

Modify

MultipleStepoverBuilder.Modify

Modify item

Signature Modify(index, numOfPasses, distance, intent)

Parameters:
  • index (int) – the index of item to be modified
  • numOfPasses (int) – the new value of num of passes
  • distance (float) – the new value of distance
  • intent (int) – the new value of intent

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

MoveDown

MultipleStepoverBuilder.MoveDown

Move down a item

Signature MoveDown(index)

Parameters:index (int) – the index of item to be moved down

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

MoveUp

MultipleStepoverBuilder.MoveUp

Move up a item

Signature MoveUp(index)

Parameters:index (int) – the index of item to be moved up

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Validate

MultipleStepoverBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.