MultiBladeGeomBuilderPartAxisOfRotationTypes Enumeration

NXOpen.CAM.MultiBladeGeomBuilder.PartAxisOfRotationTypes is an alias for NXOpen.CAM.MultiBladeGeomBuilderPartAxisOfRotationTypes

class NXOpen.CAM.MultiBladeGeomBuilderPartAxisOfRotationTypes

Bases: object

Available types for Part Axis of Rotation

Enum Members

Enum Member Enum Member Description
Zm
+ZM
Specify
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.