MultiBladeBaseGeometry Class¶
-
class
NXOpen.CAM.
MultiBladeBaseGeometry
¶ Bases:
NXOpen.TaggedObject
Represents a selectoin geometry Builder
This is an abstract class and cannot be instantiated.
New in version NX7.0.0.
Methods¶
Method | Description |
---|---|
GetFaces | Get the selection faces @return the selected faces |
RemoveFaces | Remove the faces |
SetFaces | Set the selection faces |
Method Detail¶
GetFaces¶
-
MultiBladeBaseGeometry.
GetFaces
¶ Get the selection faces
Signature
GetFaces()
Returns: the selected faces Return type: list of NXOpen.NXObject
New in version NX7.0.0.
License requirements: None.
RemoveFaces¶
-
MultiBladeBaseGeometry.
RemoveFaces
¶ Remove the faces
Signature
RemoveFaces(faces)
Parameters: faces (list of NXOpen.NXObject
) – the deselection facesNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
SetFaces¶
-
MultiBladeBaseGeometry.
SetFaces
¶ Set the selection faces
Signature
SetFaces(faces)
Parameters: faces (list of NXOpen.NXObject
) – the selected facesNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)