MillingTrackpointBuilderTypes Enumeration

NXOpen.CAM.MillingTrackpointBuilder.Types is an alias for NXOpen.CAM.MillingTrackpointBuilderTypes

class NXOpen.CAM.MillingTrackpointBuilderTypes

Bases: object

the definition enum

New in version NX10.0.0.

Enum Members

Enum Member Enum Member Description
Full
Full
ByDiameter
By Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.