MachiningFeatureGeom Class

class NXOpen.CAM.MachiningFeatureGeom

Bases: NXOpen.TaggedObject

  • This class represent the builder for machining feature geometry

New in version NX8.0.0.

Properties

Property Description
Features Returns the features
Tag Returns the Tag for this object.

Methods

Property Detail

Features

MachiningFeatureGeom.Features

Returns the features

-------------------------------------

Getter Method

Signature Features()

Returns:
Return type:NXOpen.CAM.CAMFeatureList

New in version NX8.0.0.

License requirements: None.