MachineTurretGroupBuilderMctTurrentWplTypes Enumeration

NXOpen.CAM.MachineTurretGroupBuilder.MctTurrentWplTypes is an alias for NXOpen.CAM.MachineTurretGroupBuilderMctTurrentWplTypes

class NXOpen.CAM.MachineTurretGroupBuilderMctTurrentWplTypes

Bases: object

WorkPlane Type

Enum Members

Enum Member Enum Member Description
Xy
XY
Xz
XZ
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.