MachinePocketGroupBuilderRegisterType Enumeration

NXOpen.CAM.MachinePocketGroupBuilder.RegisterType is an alias for NXOpen.CAM.MachinePocketGroupBuilderRegisterType

class NXOpen.CAM.MachinePocketGroupBuilderRegisterType

Bases: object

the register type

Deprecated since version NX8.5.0: This NXOpen.CAM.MachinePocketGroupBuilderRegisterType is no longer supported.

Enum Members

Enum Member Enum Member Description
SameAsPocketId
use same as pocket id
Specify
use specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.